Pipe Network Editor

Pipe Network Structure

Figure 1: Pipe Network Structure

The Pipe Network Editor is a tool dedicated to the description of the motion part of the application (Pipe Network Concept).

Functions of the Pipe Network Editor are accessed via context sensitive menus.

When the Pipe Network Editor is used, an ST file containing all the calls to the Motion / Pipe Network Library is automatically generated during compilation, and based on the graphical description of the Pipe Network.

Grid

The layout of the editor is grid oriented, which means that items (except the comments) are placed in the middle of a rectangular area called a grid unit.


  • Comments are not centered in the grid unit but merely placed at the cursor position.

Concept Link IconSee Also